Cancel
Showing results for 
Search instead for 
Did you mean: 

Preview looks fine, yet cannot create unbend?

Legend
Legend

Is there a way to force it to work? I don't care if the result is perfect or not

force unbend.PNG

 

I get this quite a bit converting to sheet metal or even when just creating blends. The preview shows me a visually acceptable result, yet it errors out.

Rob Newcomb, CAD/CNC/Simulation manager
Elmhirst Industries, Specializing in Prototype sheet metal stampings and assemblies

Production: NX 12.0.2 / Autoform r8 /WorkNC 2019 r1
Testing:NX 1855
PC: Rave Cadbeast: Intel(R) i7-4790K CPU @ 4.GHz /32gb ram /NVIDIA Quadro P2000 on Win10 Pro
4 REPLIES 4

Re: Preview looks fine, yet cannot create unbend? Might try global shaping

Experimenter
Experimenter

Capture.JPG

Re: Preview looks fine, yet cannot create unbend?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @R_Newcomb,

Can you provide a part that it fails on so I can take a look?

thanks

Dave

Re: Preview looks fine, yet cannot create unbend?

Phenom
Phenom

@R_Newcomb,

 

Can you try the following;

 

  • fit the complete model on your screen.
  • Start the unbend feature
  • select the stationary edge or face
  • Use CTRL-A to select all the bends (even when you only want one bend unbent)
  • OK or apply.

Does this work?

Huysmans Metalen n.v.
2x NX 12.0.2.9 Mach Designer
on Win10 64bit
NX Beta Tester with focus on Sheet Metal
Command Finder is your friend

Re: Preview looks fine, yet cannot create unbend?

Legend
Legend
I try to give that a shot this afternoon,

When I went to send the part to Gtac Saturday I wouldn't even go as far as showing me the Preview.
I ended up coming up with an alternate solution of course, but I still plan on sending this one into Dave to look at.
Rob Newcomb, CAD/CNC/Simulation manager
Elmhirst Industries, Specializing in Prototype sheet metal stampings and assemblies

Production: NX 12.0.2 / Autoform r8 /WorkNC 2019 r1
Testing:NX 1855
PC: Rave Cadbeast: Intel(R) i7-4790K CPU @ 4.GHz /32gb ram /NVIDIA Quadro P2000 on Win10 Pro