Cancel
Showing results for 
Search instead for 
Did you mean: 

Print 2A0 corrupt

Experimenter
Experimenter

Dear All,

 

I'm facing trouble about printing NX data with A0 overr size, it did not enough data ( element is lacked )

With A0 size , i can print normal

my ploter is HP T2530

Method printing via FTP

If i export to PDF file from NX and print via driver windown , it can print normal , full 1,5 A0 Size 

Please support me 

 

many thank

9 REPLIES

Re: Print 2A0 corrupt

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Just to make clear, are you:

1) File -> Print

or

2) File -> Plot

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Print 2A0 corrupt

Siemens Legend Siemens Legend
Siemens Legend

If printing PDF's works for you , keep doing that.

 

Regards,

 Tomas

Re: Print 2A0 corrupt

Experimenter
Experimenter
the trouble happen when i chose File -> Plot

So, could you have any solution for me ?

Re: Print 2A0 corrupt

Experimenter
Experimenter
we need printing in NX via plot , that why i need help Smiley Happy
have you got any solution ?

Re: Print 2A0 corrupt

Experimenter
Experimenter

Hi , I also test with chosing : File ->print , result good , have no any lack element, just only print file -> plot ( via FTP ) has trouble

Re: Print 2A0 corrupt

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Plotting configuration is set up (NX10) under "File" -> "Utilities" -> "Printer Administration" (Gotta Love NX consistancy!)

It can also be done externally to an NX session using %UGII_BASE_DIR%\nxplot\nxplotadmin.exe

 

Unfortunately there's so many params for a plot queue it is hard to figure out with just a description.

I'd guess the queue is set up a specific size and to "100%" size (not "best fit to page")

You have a bunch of options, but maybe define another paper size?  or enable "best fit to page"?

 

You may have to play around a bit to see what works.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Print 2A0 corrupt

Experimenter
Experimenter
Hello Ken_A

i still not solve that matter, can you have any solution ?
have you got some way to edit plot size in the setting?

Re: Print 2A0 corrupt

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I would suggest you work with GTAC (or your local VAR) on this.

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Print 2A0 corrupt

Siemens Legend Siemens Legend
Siemens Legend
As Ken says,
Setting up the Plot feature for NX is very complex since there are so many possible parameters,
and the combination with specific printers and corresponding drivers ...

Try speak to Gtac, and if that doesn't help, use the pdf workaround.