Cancel
Showing results for 
Search instead for 
Did you mean: 

Print scale factor not working

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hello everyone!

 

What is the trick with using Scale Factor in the Print utility? Whatever I put there, it does not change the actual line thickness on a paper sheet.

 

2017-09-26 (2).png

2 REPLIES 2

Re: Print scale factor not working

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Did you try hitting the "F1" key with the dialog open - does the context sensitive help describe more?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Print scale factor not working

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Yes, I did. "Sets the scale factor for the selected custom line width." That is less than helpful - I tried modifying the value to no effect whatsoever.