Cancel
Showing results for 
Search instead for 
Did you mean: 

Problem measuring angle

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi guys,

 

My customer is having problems in measuring angles which did not exist in NX7.5

angle.jpg

Can you help?

I believe it is getting the axis of this face and telling the angle is Zero.

 

Cem

 

7 REPLIES

Re: Problem measuring angle

Siemens Phenom Siemens Phenom
Siemens Phenom

 What angle are you trying to measure? It is not totally clear from the image

 

Steve V

Re: Problem measuring angle

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Planar face or Z vector and the cylindirical angled face that i pointed out.

Re: Problem measuring angle

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

(view in My Videos)
I've also put a video to make it easier to understand

Re: Problem measuring angle

Siemens Phenom Siemens Phenom
Siemens Phenom

Can you post this example model?  I'm struggling to understand what the 90 degrees in the initial measurement even means here.

 

Generally speaking, the angle being measured here is between the normal of the planar face and the center axis of the cylindrical face.  You can see that axis being displayed temporarily while selecting the cylindrical face, and one of the vectors in the final annotation should be aligned with this axis.  

 

And so for a planar face with a perpendicular cylinder, the angle should indeed be either zero or 180 degrees, depending on which way the normals are pointing.

 

If the cylindrical face is incluned relative to the planar face, then you should be seeing something like this, where the 70 degree measure is showing one vector normal to the highlighted planar face, and the other vector lying along the axis of the cylindrical face.

 

2016-03-25_10-35-33.png

 

Does that help?  Again, if you can send the part, I'd love to understand what they were seeing before.

 

Thanks!

 

Taylor Anderson
NX Product Manager, Knowledge Reuse and NX Design
Tel: +1 (602) 441-0683
taylor.anderson@siemens.com

Re: Problem measuring angle

Siemens Phenom Siemens Phenom
Siemens Phenom

Ok so the bug on the website is fixed so can now see attachments to messages.

The zero or 180 degree measurement result makes sense as it is measuring the angle between the normal of the plane and the axis of the conical face (extrude in same plane as planar face with 8 degree taper). To get the 8 degree measurement you will have to measure to an intenrsection curve constructed on the face, or simply Information Object commands on the face will give you half angle of a conical face.

Why earlier versions of NX were giving the 8 or 98 degree on selecting the conical face I am not sure.

 

Steve V

Re: Problem measuring angle

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Hi Steven.
Actually the NX8.5 version of the angle measurement makes more sense to me and the customer for measuring an angled face with two clicks.
Don't you think it is difficut to measure an angled face?? Creating an intersectioncurve etc...

Cem ALPAY
iPhone'umdan gönderildi

Re: Problem measuring angle

Siemens Phenom Siemens Phenom
Siemens Phenom

Change the second reference to Vector and the specify Face/Plane Normal to get the angle you need.

 

(view in My Videos)

Steve V