Cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with Zipping assembly

Genius
Genius

Hello, I'm having trouble with zipping an assembly that I'm working in and I'm not sure why.  I'll go to Menu -> File -> Zip Assembly and then select Work Park in the Pop-Up window.  I'll then select the ZIP-File "..."  and then hit OK and OK. Most of the time, this will work fine and I'll have a zipped assembly created.

On occasion, this won't happen and I'll get another pop-up window stating UG-error:  File not found.  A zip file will still be created in the specified folder, but it's only 1 KB.  This seems to be an intermittent problem and I haven't been able to figure out what's going on.  Has anyone seen this happen before?  Any recommended fixes?  Thanks

2 REPLIES 2

Re: Problem with Zipping assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Have you looked in the log file to see if there's a better details on the error?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Problem with Zipping assembly

Siemens Phenom Siemens Phenom
Siemens Phenom

@s_hightower , Does your path or part name contains any special characetrs? Or does your path + part name character count is greater than 128?

Regards,
Samadhan

GTAC | NX Help: NX1102 | NX1202 | NX1847
Please mark post as an "Accepted Solution", if it answers your question/is more helpful!