Cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with boss

Experimenter
Experimenter

I was trying to put a shallow boss on a sheet of material. The error message is "cannot unite opposed sheet bodies". I don't know what to do now.

2 REPLIES 2

Re: Problem with boss

Genius
Genius

This will help you if problem is related to the specially Unit

In order for the unite operation to be useful, the specified solids must intersect. In order to unite sheet bodies, they must meet at their edges unless they have overlapping faces.

 

obj

The target solid.

WITH

Minor word specifying that the target solid is united with the following object list.

obj list1

List of solid objects to be united with the target solid. Maximum allowed in list is 1000.

CNT

Optional minor word indicating that a count of solid objects is to be returned.

c

Variable which returns the number of solid objects.

IFERR,label:

Specifies a label to which program execution jumps if an error occurs. Possible errors include: maximum amount of objects exceeded; illegal object specified; cannot unite opposed sheets; can't unite solid with sheet, etc.

RRG

Re: Problem with boss

Legend
Legend
Hi
Most of all, Boss [Insert > Design feature > Boss] is not support Sheet body for target.
You may use Emboss command for similar results with Sheet body target. [Insert > Design feature > Emboss]

 Sunkap Ahn, Senior Support Engineer


logo