Cancel
Showing results for 
Search instead for 
Did you mean: 

Problems with Linking Attribute to expression in NX8

Valued Contributor
Valued Contributor

In NX 8 in some files after some use I can no longer link attributes to expressions. If I create a new attribute, then go to expressions and click reference part attribute I get the following error pictured below. Is there anyway to fix this. If I open the file in NX9 or 10 the problem is fixed, but unfortunately I can only use 8.

Using NX 8.0.3.4
2 REPLIES

Re: Problems with Linking Attribute to expression in NX8

Siemens Phenom Siemens Phenom
Siemens Phenom

Are you certain that an expression linking to the attribute doesn't already exist?

Taylor Anderson
NX Product Manager, Knowledge Reuse and NX Design
Tel: +1 (602) 441-0683
taylor.anderson@siemens.com

Re: Problems with Linking Attribute to expression in NX8

Valued Contributor
Valued Contributor

yes, same file opened up in a newer realease solves the issue. I assumed siemens knew about this since this is not an issue with newer realeases, but perhaps not.

Using NX 8.0.3.4