Cancel
Showing results for 
Search instead for 
Did you mean: 

Problems with the installation of NX 12.0 documentation

Experimenter
Experimenter

Hi,

 

I was trying to install the  documention file of NX 12.0 recently, but when I press the key F1, it displays an error webpage after the installtion as below:1.png

 If I broswer localhost:8282 directly, it shows another error webpage:2.png

 

 

I've tried several times to uninstall and reinstall the PLM DOCUMENTATION SERVER and the Documentation file, but it still doesn't work. 

Has anyone what causes the problems and how to fix them? Any information is appreciated.

 

Thanks in advance!

12 REPLIES

Re: Problems with the installation of NX 12.0 documentation

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Why do you want to install the NX 12 documentation?

Default it's pointing to the documentation server of Siemens.

So when you have internet acces your documentation is set fine.

 

 


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: Problems with the installation of NX 12.0 documentation

Legend
Legend

I think documentation is not installed properly.

You can use the below link for NX12 Documentation.

 

https://docs.plm.automation.siemens.com/tdoc/nx/12/nx_help#uid:index

 

:Smiley SurprisedPTIMUS_PRIME

::Smiley SurprisedPTIMUS_PRIME

Re: Problems with the installation of NX 12.0 documentation

Experimenter
Experimenter

I have to intall the NX12 documentation because sometimes I don't have access to the internet. 

Re: Problems with the installation of NX 12.0 documentation

Phenom
Phenom
Ensure your system variable for UGII_UGDOC_BASE=http://localhost:8282

Re: Problems with the installation of NX 12.0 documentation

Phenom
Phenom

Look for DelploySolrIndex.bat

 

Place your doc library .zip file in this folder. Then run the bat file.

Capture.PNG

 

Re: Problems with the installation of NX 12.0 documentation

Phenom
Phenom

Another area to check is the port number. I think it changed in NX12

Capture.PNG

 

 

 

Re: Problems with the installation of NX 12.0 documentation

Experimenter
Experimenter

Hi,

 

Thanks very much for your help and information. I checked one by  one according to your instructions, the deplyment seems to be ok, but the problem still exists.

1.png2.png3.png

Re: Problems with the installation of NX 12.0 documentation

Phenom
Phenom

I'd call GTAC or contact your Channel Partner at this point. It might be something like having to roll back your Java version or something like that. I;m running Java Version 8 Update 161.

Re: Problems with the installation of NX 12.0 documentation

Experimenter
Experimenter

Really appreciated your help. The problem has been solved.