Cancel
Showing results for 
Search instead for 
Did you mean: 

Product Design - faster way to move thru the tree

Creator
Creator

When working on a part in 7.5...Is there a way to make the next feature in the tree current (going up or down) using the keyboard arrow keys?  Using right click to make a feature current is too slow.  I don't like using the checkmarks because next thing you know, things are unchecked that you want to see.  Solidworks makes it really nice by allowing use of the arrow keys to make the next command active/inactive with a setting.  Does NX have that?  Thanks in advance.

2 REPLIES 2

Re: Product Design - faster way to move thru the tree

Siemens Phenom Siemens Phenom
Siemens Phenom

It may not use the 'arrow keys' but there are buttons to step your model forward and backward one step at a time.

 

Just open your part and toggle ON the 'Feature Replay' toolbar where you'll find the so-called VCR controls to 'Rewind', 'Fast Forward' and single stepping 'Forward' and 'Backward' your model's features.  There's also a option where you can set the time between 'frames' and automatically playback your model's creation step-by-step like a 'movie'.  What's handy is to pin open the Part Navigator panel so that you can see exactly where you are in the part history as you play it back.

John R. Baker, P.E. (ret)
EX-Product 'Evangelist'
Irvine, CA

Re: Product Design - faster way to move thru the tree

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Make first feature current: Ctrl + Shift + Home

Make next feature current: Ctrl + Shift + right arrow

Make previous feature current: Ctrl + Shift + left arrow

Make last feature current: Ctrl + Shift + End

 

You can find/modify these in the customize dialog (right click in the toolbar area and pick customize) commands tab -> keyboard... (feature replay section).