Cancel
Showing results for 
Search instead for 
Did you mean: 

Product Interface - naming

Siemens Phenom Siemens Phenom
Siemens Phenom

This is a question for those using the Product Interface functionality in their design process.

Currently it is possible to create more than one product interface with the same name. I would like to have people's feedback on this. Do you see this as an advantage or as a disadvantage?

Does anyone have a workflow process where duplicate product interface names are used?

If NX forced uniqueness of product interface name would it cause any difficulties?

 

 

Steve V
1 REPLY 1

Re: Product Interface - naming

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

I think it would cause difficulities. If a user define product interface in a conceptual part (like units' layout difinition part - sometimes named skelton part), there are some interface objects necessary for the same unit, for instance, origin - datum c-sys, boundary sheets against the other units and so on and those interface names should be the same name like "for lens unit". Does this make sense for you?