Cancel
Showing results for 
Search instead for 
Did you mean: 

Project a point on a curve/edge

Valued Contributor
Valued Contributor

Hello,

 

Is there an interactive function available which allows us to project a point on a curve/edge?

2 REPLIES 2

Re: Project a point on a curve/edge

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

If you want to create a point on the curve where the curve is at shortest distance from the input point, then create a Datum Point and choose the Point On Curve/Edge type. Select the curve and then change the Location Reference to Start Point. Enter 0 mm as Curve Length and you point is at the closest location. 

 

If you want to project inside a plane then you will have to create an intersection point between the plane and the point. 

 

Regards, **bleep**

Re: Project a point on a curve/edge

Valued Contributor
Valued Contributor

@DickBaardsethanks for the reply. I was able to project it by creating a plane by point and direction method where the point is the point to be projected and direction is the edge vector on which the point lies. Then I created an intersection point between this plane and the edge on which the point has be projected, the resultant point is the projected point.

 

I was not able to find any direct function in OOTB NX