Cancel
Showing results for 
Search instead for 
Did you mean: 

Projected distance in the new Measure command

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hello everyone!

WIth the new Measure tool, how to perfrom a measurenemt that was before known as "Projected distance"?

4 REPLIES

Re: Projected distance in the new Measure command

Siemens Phenom Siemens Phenom
Siemens Phenom

Select your two objects to measure between, then add a vector.  Use the 'Hints' text to help you.

2018-04-27 08_57_52-Measure.jpg

Re: Projected distance in the new Measure command

Siemens Phenom Siemens Phenom
Siemens Phenom

A PDF document 'NX1201_mp01_Measurements' can be found in the extracted 'nx-12.0.1.mp01' package which covers some information related to this new Measure command.

Re: Projected distance in the new Measure command

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

I surely read that PDF. It doens't answer all questions though. 

What about the old 'Points on curves' measurement? How to duplicate with the new Measure tool?

Re: Projected distance in the new Measure command

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

Hi @Scaffold,

 

Using the new Measure command, just pick two points on the curve.  NX will display two values; Minimum Distance (associative) and Points on Curve Length (non-associative).  To get the value from Points on Curve Length to the previous dialog you can either Right click and copy the value from the Points on Curve Length dialog, or check the option in the Settings called "Send Results to NX Console" to copy/paste the value as required.

 

Note that this workflow using the old Measure method was also non-associative.

 

Regards, Ben