Cancel
Showing results for 
Search instead for 
Did you mean: 

Projected section view in drawing not shown

Pioneer
Pioneer

Hey.

 

I have base in my drawing and I´m trying to make basic projected section view. Just a cutline with letters A-A appears on the baseviw, but section view itself is missing. It wont even offer to place it anywhere, after clicking the cutline on the base view.

 

All the layers are visible and all the plus icons are clicked from "show and hide".

6 REPLIES 6

Re: Projected section view in drawing not shown

Genius
Genius

Once you have created the sectional line, you can create the sectional view by other command. I dont rememeber how the command is named in english but must be something like sectional view or section view.

 

This comand can be also used to directly/quickly create section views whose section line has one or two segments.

Re: Projected section view in drawing not shown

Gears Phenom Gears Phenom
Gears Phenom

Check your settings....sounds like you have 'without Section View'

Or you are adding a Section Line not a Section View.

 

section.gif

Re: Projected section view in drawing not shown

Pioneer
Pioneer

Just a one little problem, I do not have that kind of settings in my NX9.

Re: Projected section view in drawing not shown

Gears Phenom Gears Phenom
Gears Phenom

If I remember, it's a toggle on the Dialog for Show with View in NX9

Re: Projected section view in drawing not shown

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@MikeHenry wrote:

Just a one little problem, I do not have that kind of settings in my NX9.


When placing the view, press the "settings" button

section_1.png

 

 

The setting mentioned by @joewhite will be in that dialog.

 

section_2.png

 

 


@Javiduc  wrote:

Once you have created the sectional line, you can create the sectional view by other command.


That workflow is not available in NX 9, the new section line command came about in NX 10.

Re: Projected section view in drawing not shown

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

 

 

Hi @MikeHenry 

 

It's not so obvious in NX 9.  Having defined your hinge line, right mouse click and on the popup menu you'll see that "Section Line Only" is enabled:

 

Screenshot - 8_13_2019 , 7_55_11 AM.png

 

Disable this option on the menu and your views should now show.

Ben Broad | PLM Enthusiast | Siemens GCSS

NX (v17 - 1876) | Teamcenter (9 - 12)
Value Based Licensing | Adaptive UI | BETA Registration