Cancel
Showing results for 
Search instead for 
Did you mean: 

Punch a text in sheet metal enviroment

Builder
Builder

Hello,

 

I have not to much experience in Sheet metal Enviroment and I need some help. How can I to punch a text into a sheet of metal?  I've used  text command following with insert/punch/bead.

It apears an error: "section should not contain a B spline curve with sharp corners"

Thanks for your help.

Jose C

4 REPLIES 4

Re: Punch a text in sheet metal enviroment

Siemens Phenom Siemens Phenom
Siemens Phenom

You need to use a single stroke text font.  Use 'Modern'.

Re: Punch a text in sheet metal enviroment

Siemens Phenom Siemens Phenom
Siemens Phenom

I should have added that there can be no 'corners' on the text.  You may need to work on the text curves to get them smooth and tangent.

Re: Punch a text in sheet metal enviroment

Builder
Builder
Thanks for your reply. Definitely I need to work on the text curves. With "modern Font" only Works on letters with straight sections and not with curves like, C, S, etc

Regards

Jose C

Re: Punch a text in sheet metal enviroment

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You may need to define your own font

I would suggest using Fontforge, but there are others as well.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled