12-09-2017 02:14 AM
I have been trying different thing but all in vain
without that option life has become miserable I have to deselect and select again and I have to do that repeatedly.
Someon please help me out here
USING NX11.0.0.33
Solved! Go to Solution.
12-09-2017 10:53 AM - edited 12-09-2017 10:54 AM
Ciao,
I don't have this license at home so I could be imprecise. Activate More options as I show you in the attached image.
It should appear the flag 'deselect automatically'.
I hope it is what you need.
Ciao
12-09-2017 08:45 PM - edited 12-09-2017 08:46 PM
Namaste,
Thanks Cesar, I looked into that but that is already set to 'more'....
Anything else I can try?
12-11-2017 09:19 AM
On selection toolbar the command to turn it off and on is there. It is also then on the mini-selection toolbar and I am only showing it on the selection toolbar.
Scott
12-11-2017 09:23 PM
Namaste,
You are a Life Saver. Thanks
12-12-2017 01:36 PM
Namaste,
the pic which you have sent, I can see that when you hover your mouse cursor over the command, it shows the little dialogue box where command and what it does is shown.
However in my case, I can only see the command only.
12-13-2017 07:21 AM
If you hit (CTRL)+1 you get the menu to customize the layout, Do you have tooltips turned on?
Tooltips turned on
Scott
12-13-2017 07:48 AM