Cancel
Showing results for 
Search instead for 
Did you mean: 

Radial Menu not functioning properly

Valued Contributor
Valued Contributor

Hello folks,

 

We have to start working with NX10 now.

The radial view menu (press RMB a long time or move-press RMB) always had the static wireframe view mode. But now it is gone.

If I modify that menu via customize (ctrl 1) the modified radial menu just holds for a very short time. My modifications are gone very soon.

How to keep my modifications permanently?

 

We use NX 10.0.3.5

 

Many thanks for your help.

4 REPLIES

Re: Radial Menu not functioning properly

Siemens Phenom Siemens Phenom
Siemens Phenom

It can be done 2 different ways. 

 

The first thing to do is setup the screen and menu buttons to what you want them to be and then save a role to keep them. I do it this way.

 

The other thing is to make sure the save layout on exit is turned on in the Preferences->Interface menu.

 

Scott

Re: Radial Menu not functioning properly

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello @Blendy,

 

Have a look at this recent newsletter Article, it explains the problem you are encountering:

 

Adding-Static-Wireframe-back-to-the-radial-dialog.docx - NX

 

Kind regards,

 

Dennis

Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software

Re: Radial Menu not functioning properly

Legend
Legend

are you running the latest MP for 10.3.5?

 

you lose it when you pop in and out of sketcher and or drafting correct? I think they fixed it around mp06 or7

 

Rob Newcomb, CAD/CNC/Simulation manager
Elmhirst Industries, Specializing in Prototype sheet metal stampings and assemblies

Production: NX 11.0.2.7 / Autoform r7 /WorkNC 2017 r2
Testing:NX12 EAP
PC: Rave Cadbeast: Intel(R) i7-4790K CPU @ 4.GHz /32gb ram /NVIDIA Quadro K2200 on Win10 Pro

Re: Radial Menu not functioning properly

Valued Contributor
Valued Contributor
That problem is apparently solved now. We just installed the latest Patch 10.

Many Thanks!