Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Radius arrow settings don’t adhere

Phenom
Phenom

I would like to see the radii dimension arrows’ Stubs at the opposite side and therefore edited them with Setting>>Line/Arrow ->Stub-Orientation.

Now I would like to re-position slightly those radii dimensions. As soon as I move them, they jump back to default as before. How could I force to have settings as edited?

 

Michael Fernando


Die Designer
NX 11.0.2.7 + PDW

4 REPLIES 4

Re: Radius arrow settings don’t adhere

Siemens Phenom Siemens Phenom
Siemens Phenom

Try holding down the CTRL key when you move the radial dimensions.  This should maintain the stub orientation.

Re: Radius arrow settings don’t adhere

Phenom
Phenom

Yes, Ctrl locks the jumping back to default settings.

 

Another issue: Unable to “Inherit” the new Radius settings to another R dimension thru Setting Source=selected object.

 

I assume that you are working at NX. Would it be possible to give more editing power to the arrow handles? It’s time consuming to edit with windows.

 

Michael Fernando


Die Designer
NX 11.0.2.7 + PDW

Re: Radius arrow settings don’t adhere

Siemens Phenom Siemens Phenom
Siemens Phenom

If you want to see some improvements in functionality, you will need to contact GTAC.

Re: Radius arrow settings don’t adhere

Siemens Phenom Siemens Phenom
Siemens Phenom

What version of NX are you running?

John R. Baker, P.E. (ret)
EX-Product 'Evangelist'
Irvine, CA