Showing results for 
Search instead for 
Do you mean 
Reply

Reference Mapping when adding UDF

I made a UDF that required a point to specify its location. When I made the UDF I selected the point one time. There are other conditional features but I never selected the point to produce those features.

 

When I add the UDF, I resolve three external references, a point and two planar surfaces, then a Reference Mapping dialog appears (see attached) that, I'm guessing, is mapping a point to a point. I can click OK and the UDF appears to go in fine. But it's presence is still most annoying. Anybody know what this is and why it appears? 

2 REPLIES

Re: Reference Mapping when adding UDF

It's showing that the UDF Reference is not given properly. Share me the UDF file. I will try to fix my level best.

Re: Reference Mapping when adding UDF

Hello,
I have the same issue.
Could you share your solution? Do you find out where was the problem?