Cancel
Showing results for 
Search instead for 
Did you mean: 

Remove assigned material

Phenom
Phenom

Hi, 
how remove material from a body assigned by the command assign material?

Thank you...

Using NX11 and NX1847
RuleDesigner PDM

2 REPLIES

Re: Remove assigned material

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Go to Manage materials (local materials) -> select the material from the list and press the "delete selected materials" button.

Re: Remove assigned material

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor
Cowski's solution is good for pre-NX11.

In NX11 the icons have been removed. Select "Menu > Tools > Materials > Manage Materials". You can either use the default "Library Materials" or select the Library Materials pull down and choose "Local Materials". Right click the material with the green check mark that you want to unassign and choose "Remove Usages".

If you don't intend using the material you can right click the material and choose Delete to remove it from your list of Local Materials. Otherwise you can keep it in your Local Materials, should you wish to apply it to other bodies.

Regards, Ben