Cancel
Showing results for 
Search instead for 
Did you mean: 

Remove overlap entities

Phenom
Phenom

Hi,

I've imported a DXF file into a part. There are much overlap entities. I didn't found a specific command to remove overlap entities. Have you a solution to clean this situation ?

Thank you...

Using NX11 and NX1847
RuleDesigner PDM

7 REPLIES

Re: Remove overlap entities

Phenom
Phenom

Use again DXF/DWG Export Wizard and under Options’ Options there is “Remove Overlapping Entities” to select.

Michael Fernando


Die Designer
NX 11.0.2.7 + PDW

Re: Remove overlap entities

Phenom
Phenom

@mike_fdo wrote:

Use again DXF/DWG Export Wizard and under Options’ Options there is “Remove Overlapping Entities” to select.


This option I know, but import...modify part...discover overlap entities....export again, import again...

Useless works.

Nobody has a journal to clean this situation ?

Thank you...

Using NX11 and NX1847
RuleDesigner PDM

Re: Remove overlap entities

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If you are using NX 10 or above, you can use "optimize 2D curve" to remove duplicate entities.

Re: Remove overlap entities

Phenom
Phenom

@cowski1 wrote:

If you are using NX 10 or above, you can use "optimize 2D curve" to remove duplicate entities.


I've NX10 and used this command, but doesn't cleaned overlap entities, for this reason I open a topic on the forum.

Thank you...

Using NX11 and NX1847
RuleDesigner PDM

Re: Remove overlap entities

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

That would have been good information to add to your opening post...

Re: Remove overlap entities

Phenom
Phenom

@cowski1 wrote:

That would have been good information to add to your opening post...


Hi,

sorry but english is not my language and when I think to open an IR or a topic I snort...

Thank you...

Using NX11 and NX1847
RuleDesigner PDM

Re: Remove overlap entities

Builder
Builder

hello guys

 

 

i also face this problem

 

i inserted dwg file in nx part & modified model

 

when i inherit PMI fonts automatically changed

also in drafting 

 

& when do drafting dimension not getting 

proportionate to views

Decimal.JPGCant control decimals in drawingDecimal_01.JPGDimesion not proportionate to viewDecimal_02.JPGCant control decimals in drawing

Warm Regards
Thomas Roman
Machine Designer