Cancel
Showing results for 
Search instead for 
Did you mean: 

Removing extra sheet no.from drawing ?

Valued Contributor
Valued Contributor

Hi

When printing title block indicates "SHEET NO. 1-2". (=1st sheet out of 2 available = 1/2)

  • But it only has one(1) sheet in NX drafting.
  • Someone has deleted the second sheet inside NX some years ago and now the "page/sheet 2" just haunts there...when outputting prints and pdfs. How to remove it from prints ?date.jpg
3 REPLIES

Re: Removing extra sheet no.from drawing ?

Esteemed Contributor
Esteemed Contributor

It depends how it is defined.

Edit the text, is it hardcoded to "2"?

Or does it point to the drawing sheet attribute:

<W@$SH_NUMBER_OF_SHEETS>

 

 

If the former, change to the latter (or just change to "1")

If the latter, it is probably a bug and should be reported to GTAC

If something else, then I don't know.

 

Ken

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP5 + patch/TC11.2
I'd rather be e-steemed than e-diseaseled


Re: Removing extra sheet no.from drawing ?

Valued Contributor
Valued Contributor

 

titleblockgfgf.jpg

It says this. How can I enter to sheet attributes/Edit text ?

Re: Removing extra sheet no.from drawing ?

Valued Contributor
Valued Contributor

It is a problem in NX8.5.3, also. I thought it was reported to GTAC at that time. I use the drawing sheet attribute. I usually change parts then go back to original, and it clears up. Sometimes it takes 2-3 tries for it to fix itself. Not a good solution, but otherwise manually change it and don't use the attribute supplied. Either solution is a waste of our time, but is all that is available. I thought it would have been fixed by NX11 release.