Cancel
Showing results for 
Search instead for 
Did you mean: 

Replace Component for Drafting

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hi ,

 

im a bit desperated. In NX11 with TC 11.2  i wanted to replace a component below my drafting. i read a bit in the forum and found out something has changed, a lot of workarounds but none worked for me.

 

So i try to explain with the example i made here

 

replace_1.jpgBase Drawing

No i want to replace the Component. So i selected the *160 3D modell Part an made right click, replace component. 

 

replace_2.jpgReplace Component over context menu

 

I Browse for the New Component ( or opend it before and select it makes no difference) and select it

 then i recive this massage all the time, even if i change any setting it makes no ******* difference

 

replace_3.jpgMessage of hell

 

I dont know what i do wrong... Even the NX help does not provide me any solution.

 

Even if i do it in the modelling , drafting. if i made a new part, a saved as from the previous... evrytime the same ....  even another revison is not working.

 

 

Any idea where i can learn this function... because in the past it worked fine. Never change a running system.

 

 

 

1 REPLY 1

Re: Replace Component for Drafting

Solution Partner Legend Solution Partner Legend
Solution Partner Legend
god **bleep**

found it myself after i wrote the post... first close the **bleep** part then it works.