Cancel
Showing results for 
Search instead for 
Did you mean: 

Replace Text parts of Notes

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Dear Community,

 

i tried to do something special :-). I ´got a lot of notes on a drawing. and now i recognized i did a mistake that i worte the wrong letter and now i want to change all these letters from one to anoterh.  EXP. The X must be changed to 4

 

x TEST x = 4 Test 4

 

In Other tools you can allways use CTRL+H and Replace the text or a part of the text.

 

Any Ideas for NX??

 

Using Version NX10

5 REPLIES

Re: Replace Text parts of Notes

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Never heard of replacing specific texts inside NX. Smiley Happy

 

Want to try export or copy and paste your notes to an external tools (MSOffice),

CTRL+H and replace the texts that you need?

then paste import or paste it back to NX? Smiley Very Happy

Re: Replace Text parts of Notes

Solution Partner Genius Solution Partner Genius
Solution Partner Genius
Jepp thx, thats a way i can handle it :-)

I also never heard of it but now it is needed :-)

Re: Replace Text parts of Notes

Siemens Phenom Siemens Phenom
Siemens Phenom

Although it has already been answered ...still just assuming if you have lot of annotations (you wish to alter)...Create a dummy Table inside drafting ...copy the annotation text inside the table cells...and once you are done use edit using spreadsheet for the table...replace the text and copy the altered text back to the annotations....

Not sure this post adds any further value to what has already been stated.

Best Regards

Kapil Sharma

 

Re: Replace Text parts of Notes

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

FrankSwinks posted some journal code on eng-tips that should help with text search and replace:

http://www.eng-tips.com/viewthread.cfm?qid=311028

Re: Replace Text parts of Notes

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

GYs you are all Awsome

 

that script is the solution and it works