Cancel
Showing results for 
Search instead for 
Did you mean: 

Replace only one occurrences with a different revision.

Legend
Legend

hi

 

We use NX 10 togheter with Teamcenter 10.1.6.

There is a request to use different revisions in same assembly.

Is it possibile within NX to replace one occurance of an item with a different revision?

 

When using Replace function I get this alert that all occurences will be replaced..

2016-10-04_15-13-43-738.png

 

Jörgen Mähler, PLM Lead Hydro
TC11.5 | TcIC11.5 | Swim 11.4 | Supplier Collaboration
NX 11,12 | Catia V5 | Solidworks 2018 | AutoCad2018
3 REPLIES

Re: Replace only one occurrences with a different revision.

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

You need to enable Multiple Revisions in your NX Customer Defaults:

 

multiple_revisions.png

 

Regards, Ben

Re: Replace only one occurrences with a different revision.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

But why do this?

How is purchasing (or supply chain) going to order "5 part ABC123 version A, and "one part ABC123 version 0"?

 

Seems like you could cause a LOT of confusion...

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Replace only one occurrences with a different revision.

Legend
Legend

Hi

 

I as admin also was curious why our engineers wanted this but it's during the development phase they use it to be able to load previous revisions as references. we have A, B and C as major revisions and this is used in A and B. C which is production maturity level they will only use one revision in the assy.

 

One alternative that I find better is to generate a new part number if there are different proposals in the loop. This makes it more easy also in A and B phase,  as to order a prototype I find it better to use 1234/B01 and 1255/B03 instead of 1234/B01 and 1234/B03.

... so we will see if I can turn the tanker around.

 

Either way it's anyway good that they can load in another revision into the assembly as well so they were satisfied yesterday.

Jörgen Mähler, PLM Lead Hydro
TC11.5 | TcIC11.5 | Swim 11.4 | Supplier Collaboration
NX 11,12 | Catia V5 | Solidworks 2018 | AutoCad2018