Cancel
Showing results for 
Search instead for 
Did you mean: 

Reset button in dialog menus

Genius
Genius

Is there a way to hide the reset button that is near the quit button? The reset button is also placed in the dialog options and I would prefer not to have it so close to the quit button where sometimes I accidentatly press it.

1 REPLY

Re: Reset button in dialog menus

Siemens Phenom Siemens Phenom
Siemens Phenom

There is no such preference/setting available to hide 'Reset' icon of a dialog (At least in NX 10).

 

I would suggest to use the keyboard/mouse to control, Use 'ESC' to discard the changes and close the window. 'MMB' to advance to the next selection step/accept the changes.

 

Regards,
Ganesh Kadole
#IngenuityIsNX | NX - What's New