Cancel
Showing results for 
Search instead for 
Did you mean: 

Reusable Component Bitmaps

Experimenter
Experimenter

Hello,

Anyone know if it's possible to use more than two bitmap on the " Add Reusable Component" interface?

If the component has a lot of paramenters, with only 2 image is difficult to understand the parameters.

 

I've found the way to use 2 images, the first pointed in the excel file associated to the component and the second in the krx.

 

Anyone know if there is a way to use more than 2 bmp.

 

Thanks for any suggestion.

 

Massimo.

1 REPLY 1

Re: Reusable Component Bitmaps

Experimenter
Experimenter

Hello Massimo,

to add more than one picture to the reusable component, you can add following synax to the Excel-File.

 

BITMAP ./picture1.bmp, ./picture2.bmp, ./picture3.bmp

 

Best regards,

Christian