Cancel
Showing results for 
Search instead for 
Did you mean: 

Reuse Library associativity

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hello everyone!

 

I'm really curious to know the reasons behind the decision to exclude support of associative paste operation for the Face and Body object types in the Reuse Library. Surely, we can build CSYS/sketch-based body and paste it associatively (provided some not very obvious conditions are met), but beyond that Reuse Library is seriously lacking. It provides robust tools to define bodies and faces based on the model but then... You can only paste them non-associatively. Is there any significant reason behind that?

 

4 REPLIES 4

Re: Reuse Library associativity

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

It would be a great enhancement to have the reuse paste associtive to the parent body.

Re: Reuse Library associativity

Phenom
Phenom

We can ask to @BenBroad if exist an already ER to be linked, if not, you can create one and share here the ER number so we can ask to be linked using GTAC support.

Thank you...

Using NX1876
RuleDesigner PDM

Re: Reuse Library associativity

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

yes, let me know if Ben has one in the system, if not, I can start ER.

Re: Reuse Library associativity

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

@Reese_Shearer wrote:

yes, let me know if Ben has one in the system, if not, I can start ER.


ER 2221648: "Add associative option to paste of reuse component".

 

Note that the above ER only covers reuse component.  A new ER will need to be opened for other object types.

 

Regards, Ben

Ben Broad | PLM Enthusiast | Siemens GCSS

NX (v17 - 1876) | Teamcenter (9 - 12)
Value Based Licensing | Adaptive UI | BETA Registration