Cancel
Showing results for 
Search instead for 
Did you mean: 

Reuse Library is slow

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

I'm working with NX 8.5 and Teamcenter.

 

We are going the create a custom component library. In the end we want to have everyting in part families (for the fastners)

But in the beginning we are going to use the existing data.

 

For example a have a hex bolt from iso 4014 in 80 different items (this will be in the future members from the part family)

When i open the folder of the library, where all the different items are in, it will take some time before this is displayed.

 

Is this because of NX in combination with teamcenter?

is there a way to load the components fasters in the member select preview?

 


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions
7 REPLIES 7
Highlighted

Re: Reuse Library is slow

Siemens Phenom Siemens Phenom
Siemens Phenom

In general, it is not the combination of Teamcenter and NX that affects performance.

 

It is normal for the 'first' load of the reuse library to be slower than subsequent loads.  NX caches some data during the 'first' load. If the reuse library is accessed again, the loads should be faster.

 

There have also been cases where the parts in the reuse library were saved in a previous version of NX.  Conversion to the latest version during load takes additional time. Opening the files in the version of NX you are using, then saving them would speed up the load process.

 

Finally, I believe that improvements have been made to the way the reuse library is handled in newer versions of NX.

Re: Reuse Library is slow

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Thanks for the respons!

 

That makes things clear.

We are preparing to upgrade to NX11 so i hope that the speed there is better.


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: Reuse Library is slow

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Ruud,

 

If you are going to NX 11.0, you might also want to have a look at indexing your reuse library.

 

There is more to it, but have a quick look at this FAQ:

http://solutions.industrysoftware.automation.siemens.com/view.php?si=002-7008572

 

Kind regard,


Dennis

Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software

Re: Reuse Library is slow

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Dennis,

I have recently installed the index search on my own machine.
works nice!


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: Reuse Library is slow

Phenom
Phenom

@Ruud_vandenbrand wrote:
Dennis,

I have recently installed the index search on my own machine.
works nice!


Hi Dennis,

index library works for search reuse components, not on open or expand folder library in the resource bar.

Thank you...

Using NX11 and NX1847 serie
RuleDesigner PDM

Re: Reuse Library is slow

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
That's right but the index on it's self is working nice.

Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: Reuse Library is slow

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello @cubalibre00,

 

If I remember it correctly, I believe from NX 11.0 it also does something for browsing the folders. But I could be slightly of here:

2017.01.20_14h07m26s_002_.png

 

Kind regards,

Dennis

Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software