Cancel
Showing results for 
Search instead for 
Did you mean: 

Revisted drawing to find all curves from model missing

Pioneer
Pioneer

This is the second time this has happened now.  The model is only showing hidden lines for what I've changed since the drawing was last updated.  Any object/hidden lines that were previously shown are not displaying.  Any advice other than what I've checked below?

 

Things I can say:

-The views are all updated.

-I can see the solid when I switch to modeling.

-Everything is on the same visible layer.

-There are no view dependent edits

-Monochrome doesn't change anything

-The drawing is in the same file as the model

-If I switch the view to fully shaded, it shows it... switching back to wireframe shows exactly what I started with.

-I've cleaned the model, tried opening it on another system running the same version.  I can't open it in an earlier version.

 

Note: The drawing was modified a few months ago in the same version and everything was fine.

 

NX 9.0.3.4

WIN 7 64-BIT
NX9.0.3.4
2 REPLIES 2

Re: Revisted drawing to find all curves from model missing

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Did you check the view(s) "layer visible in view" (I don't think  that's the problem, but you could check)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Revisted drawing to find all curves from model missing

Pioneer
Pioneer

Apparently, show>select all command in drafting, select all fixed the problem.  Thanks though for making me try some other things in the process.

WIN 7 64-BIT
NX9.0.3.4