Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Revolving edges that are not on same plane creates sheet body, I want a solid body

Gears Phenom Gears Phenom
Gears Phenom

I'm trying to revole some edges of a solid body but these edges are not all on the same plane. Because of this the result is a sheet body, but I want a solid body. How can I get a solid body from this operation?

Graham Inchley Snr R&D Engineer (Systems Development), Sandvik Coromant
Dell 7530 Precision, Win10, 32GB. Developing in: Java | C | KF
Production: [NX12.0.2 MP1]
4 REPLIES 4

Re: Revolving edges that are not on same plane creates sheet body, I want a solid body

Gears Phenom Gears Phenom
Gears Phenom

Your file appears corrupt so I can not understand exactly what you want.
Try with the selection option Face Edges.

 

Ciao

Re: Revolving edges that are not on same plane creates sheet body, I want a solid body

Gears Phenom Gears Phenom
Gears Phenom

Hmm.. 7Zip seemed to store the file with no name or something.

Anyway I've attached a WinZip file instead..

Graham Inchley Snr R&D Engineer (Systems Development), Sandvik Coromant
Dell 7530 Precision, Win10, 32GB. Developing in: Java | C | KF
Production: [NX12.0.2 MP1]

Re: Revolving edges that are not on same plane creates sheet body, I want a solid body

Gears Phenom Gears Phenom
Gears Phenom

Select the three faces with the option Face Edges, see image.

 

Ciao

Re: Revolving edges that are not on same plane creates sheet body, I want a solid body

Gears Phenom Gears Phenom
Gears Phenom

Wow. Why does that work and simply picking the boundary edges not work??

I'll mark your answer as the solution, but I'm not sure it will actually solve my overall problem:

 

The actual revolve in question is inside a UDF which I add using some NXOpen code. During the add of the UDF I have to specify the geometry to produce the revolve, Currently I pass in a single spline that defines the outer profile similar to my example part. I'm not sure how I can pass in FaceEdges...

I'll have to investigate that.

 

Thanks anyway, it might get me to a solution in the end.

Graham Inchley Snr R&D Engineer (Systems Development), Sandvik Coromant
Dell 7530 Precision, Win10, 32GB. Developing in: Java | C | KF
Production: [NX12.0.2 MP1]