Cancel
Showing results for 
Search instead for 
Did you mean: 

Robot Control on Linux: memory access violation

Experimenter
Experimenter

Hi

 

I am having an issue with the Robot Control command causing memory access violations on Linux.

 

The error is constant with NX 11 and NX 12 with both Redhat and Suse Linux.

 

Reproduce the error:

 

New Manufacturing file

Set one of the Robots from the Library

Run the "Robot Control" command

 

You are presented with the following message and the controls do not appear:

"Internal error: memory access violation"

 

Is this a know issue?

 

Thanks