Cancel
Showing results for 
Search instead for 
Did you mean: 

Rotating Intersection Curves

Pioneer
Pioneer

I am trying to draft a complicated flange surface in NX and unfortunately the draft function isn't cooperating, so my plan was to create numerous intersection curves using planes and my current flange surface, rotating the intersection curves by the desired draft angle and then create my drafted surface, but I'm running into difficulty rotating the intersection curves - if I select edit/sketch curve/move, I'm unable to select the intersection curve and move object doesn't move curves, so my great plan is currently dead in the water - any suggestions?

 

Thanks

 

Robert

 

2 REPLIES 2
Highlighted

Re: Rotating Intersection Curves

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

"and move object doesn't move curves"

 

It will if you turn off the "associative" option.

Re: Rotating Intersection Curves

Pioneer
Pioneer
Brilliant - exactly what I was after - thank you.



________________________________________________________________________________
This e-mail and any attachments may contain technical data, proprietary
information, and/or copyright material, the use of which may be restricted by
the International Traffic in Arms Regulations (ITAR), the Export Administration
Regulations (EAR), and/or export control regulations of other countries under
which export or re-export may be prohibited by law. As the recipient, you are
responsible to ensure that usage or transfer of this document or its attachments
complies with all relevant laws or regulations.