Cancel
Showing results for 
Search instead for 
Did you mean: 

Routing or piping light

Phenom
Phenom

Hi,

I've listen that exist a license of Routing or piping light ?

Thank you..
Using NX1880 and RuleDesigner PDM

Built-in functions for converting units of measure

3 REPLIES 3

Re: Routing or piping light

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @cubalibre00 ,

 

I just checked for lighting related any license call and couldn't find one.

Found around 21 license calls related to routing.

There exists a routing_piping call though, but I think this is not you're interested in. 

Regards,
Samadhan

GTAC | NX Help: NX1102 | NX1202 | NX1847
Please mark post as an "Accepted Solution", if it answers your question/is more helpful!

Re: Routing or piping light

Phenom
Phenom

Our sales man from Siemens :

 

NX Routing Base [NX30154]

NX Routing Base provides core capabilities used by all NX Routed System products. This includes all of the general capabilities to create, edit copy and move paths. Also, the capabilities to define standard part libraries and then to select parts from the library and intelligently place the parts within the paths. And finally the ability to define standard stock specifications and assign those specification to paths.

 

In the MACH 2 there is the Routing Base.

Exist also as separated license to put on-top on MACH1.

Thank you..
Using NX1880 and RuleDesigner PDM

Built-in functions for converting units of measure

Re: Routing or piping light

Siemens Genius Siemens Genius
Siemens Genius

Hello all,

Let me clarify.

 

If you are using Mach bundles, the routing_base license bit is included in NX12100, NX13100, and NX13300.

You need one of those Mach bundles for the Routing Base capability.

 

If you are using the older a la carte licensing, then you can purchase the Routing Base NX30154.  This is only available for a la carte licensing.  If you are a Mach customer, you cannot add this.  A Mach bundle with routing_base is required.

 

The routing_base license is a prerequisite for all the full routing licenses, like NX Routing Harness, or NX Routing Piping and Tubing.

 

Thanks.

Doug