Cancel
Showing results for 
Search instead for 
Did you mean: 

SELECT ALL INSTANCES OF A PART IN AN ASSEMBLY AND SUBASSEMBLIES

Genius
Genius

Is it possible to select all instances even if they are in different subassemblies in order to replace them?

6 REPLIES 6

Re: SELECT ALL INSTANCES OF A PART IN AN ASSEMBLY AND SUBASSEMBLIES

Phenom
Phenom

I would follow:

Find Components->Click on a part->OK

On the Assembly Navigator area, RMB and select “Expand to selected”

On top of a highlighted component, RMB and select “Replace Component…”

Michael Fernando


Die Designer
NX 11.0.2.7 + PDW

Re: SELECT ALL INSTANCES OF A PART IN AN ASSEMBLY AND SUBASSEMBLIES

Siemens Phenom Siemens Phenom
Siemens Phenom

Menu > Assemblies > Context Control > Find Components...

 

There you can use the various options available. Most easy is 'From List' tab, select the required component and hit OK. It will select and highlight all the instances in ASN and UI.

 

Re: SELECT ALL INSTANCES OF A PART IN AN ASSEMBLY AND SUBASSEMBLIES

Siemens Phenom Siemens Phenom
Siemens Phenom

Another way is to use 'Name Selection' filter from Selection group.

 

name selection.pngname selection.png1.png

 

 

Re: SELECT ALL INSTANCES OF A PART IN AN ASSEMBLY AND SUBASSEMBLIES

Genius
Genius

Thank you all. It will save me a lot of time when importing assemblies to TC and I want to replace some newly imported screws, nuts... by the ones I already have in the database.

Re: SELECT ALL INSTANCES OF A PART IN AN ASSEMBLY AND SUBASSEMBLIES

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

"It will save me a lot of time when importing assemblies to TC and I want to replace some newly imported screws, nuts... by the ones I already have in the database."

 

Or, you could change the import option for those parts to "use existing" and specify which part in the database to use, thus avoiding the need to replace components later...

Re: SELECT ALL INSTANCES OF A PART IN AN ASSEMBLY AND SUBASSEMBLIES

Genius
Genius

I think I cant. The id is the key field, is numeric and automatic and do not match the name of the file.