Cancel
Showing results for 
Search instead for 
Did you mean: 

STEP FILE TRANSLATION ISSUE

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello all,

 

 

  One of my customer is facing an issue while exporting to stp. The issue is whenever he creates a new part and tries to export it was exporting successfully without any issue the problem comes whenever he opens a .prt file of old files in the export step translator window error comes C++ exception and only log file was coming as output but not stp file and this happens only on old files.

 

 

Any suggestions how to clear this issue!

25 REPLIES 25

Re: STEP FILE TRANSLATION ISSUE

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @karthik6,

If possible, try to export STEP using same part files on another machine having the same version of NX. Otherwise, I would suggest to log an IR to GTAC with necessary log, part files.

Re: STEP FILE TRANSLATION ISSUE

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Hi Ganesh,

Thanks for the prompt reply .Yes I've tried in my machine it is exporting properly.But whenever i try in their PC C++Exception Caught will appear in log file and it happens only with old files.


Ok, I'll try Smiley Happy

Re: STEP FILE TRANSLATION ISSUE

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

It's a know problem, that is currently being fixed.

My understanding is that it's related to a Windows Update.

 

Workaround is the use File -> Save As and at the bottom of the dialog, then change the file type to STEP.
Once the type is specified, you can use the Options button to specify any settings required.
 
 
Anthony Galante, Senior Support Engineer
PhoenxPLM
24 versions of NX installed: NX4 to NX12, plus TC11.2

Re: STEP FILE TRANSLATION ISSUE

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Thank you,, i will try that

Re: STEP FILE TRANSLATION ISSUE

Experimenter
Experimenter

Hello,

 

I have the same problem with NX11 with windows 10. However, I have no problem with a windows seven installation.

Olivier G

Re: STEP FILE TRANSLATION ISSUE

Creator
Creator

I had the same problem, I have solved (temporarily) it by installing  http://www.nvidia.com/download/driverResults.aspx/123914/en-us

nVidia driver.

 

this is a solution gave to me by @cubalibre00

Re: STEP FILE TRANSLATION ISSUE

Creator
Creator

and also thanks to @BenBroad for the information he gave me about nVidia driver update

Re: STEP FILE TRANSLATION ISSUE

Phenom
Phenom

Has this issue been fixed?  Running into this same issue with NX11.0.2 mp4?

 

Thanks

 

Shane

Re: STEP FILE TRANSLATION ISSUE

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor
Has this issue been fixed? 

Microsoft has the following page which seems to reflect what users have done so far to correct this issue: Update drivers in Windows 10.  Google results reveal that this is not a new problem.  We're still collecting information, so I hope to have something more concrete to share soon.

 

Regards, Ben