Cancel
Showing results for 
Search instead for 
Did you mean: 

STL Export

Experimenter
Experimenter

Hi all,

 

I have a big problem, i use NX for 3D print modelling too, but sometimes when i export to STL the exported file contains zunds of triangles that are have the same endpoint. The problem is with it that the printer makes more material on this places. is there an option, to set the STL export that i can limit the side lenghts of the triangles?

7 REPLIES 7

Re: STL Export

Siemens Phenom Siemens Phenom
Siemens Phenom

Re: STL Export

Experimenter
Experimenter

@kapilsharma wrote:

There are some settings available https://docs.plm.automation.siemens.com/tdoc/nx/11/nx_help#uid:xid1128422:index_rapidprototyping:xid...

Best Regards

Kapil


The link you provided got this:


Error: content not found UID: xid1205322 UID Path: xid1128422:index_rapidprototyping:xid1206569:xid1205322 Sub ID: null

Re: STL Export

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

The link works fine for me (perhaps other can validate the same)

You can use the CHORDAL TOLERANCE in NX11.0.1 and Triangle Tolerance  and Adjacency Tolerance prior to NX11.0.1 for controlling the triangulation.

Does it work for you? Do let us know.

Best Regards

Kapil

Re: STL Export

Gears Phenom Gears Phenom
Gears Phenom

Link was fine for me.

Graham Inchley Snr R&D Engineer (Systems Development), Sandvik Coromant
Lenovo ThinkPad W540, Win7, 16GB. Developing in: Java | C | KF
Production: [NX8.5.3.3 MP11 64bit] Testing: [NX12.0.2 MP1]

Re: STL Export

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The first link is broken for me. I see the same error message as the OP.

The second link works...

Re: STL Export

Valued Contributor
Valued Contributor

Re: STL Export

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

It must be the space at the end of Kapil's link.  URL encoding replaces the space with "%20" and that url does not exist in the documentation - hence the error.  You can use F12 in the browser to open the console window and interrogate the html.

 

Oddly enough when Tauform quoted the text the space was removed (unless he removed the space).

The quirks of the Lithium forum application.

 

Regards, Ben