Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

STP export error

Experimenter
Experimenter

Hi together,

 

this is Chris.

 

I have a problem when I try to export an assembly as stp file.

Even when I try to export it as iges I get the same error.

 

I was searching online for a solution but couldn't find anything.

 

The log file is attached.

I hope sombody can help me to fix this issue because I need to send out the stp file asap.

 

I am using NX8.5 on Win 10 Pro.

 

since last windows update I was still able to export. Only this file don't seam to work.

 

Thanks for your help.

 

 

4 REPLIES 4

Re: STP export error

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Edifier_Chris ,

 

I see many IRs for this error whicch are fixed in NX903 and also in NX8.5 patch.

Are you on NX8.5 latest patch?

If possible attach a part file so that we can see where issue is fixed.

 

Regards,
Samadhan

GTAC | NX Help: NX1102 | NX1202 | NX1847
Please mark post as an "Accepted Solution", if it answers your question/is more helpful!

Re: STP export error

Experimenter
Experimenter

Hi @SamadhanGaikwad ,

 

I attached a picture with the system informations.

The file I can't send because it is high confidential.

It seams that this error is only at the top assembly.

If I export a sub assembly I don't get this error.

 

Also save as will have the same error.

 

regards Chris

Re: STP export error

Experimenter
Experimenter

Hi @SamadhanGaikwad ,

 

it is for sure the top assembly I found out now.

 

I created a new assembly under the top one and moved all parts and sub assemblies inside.
The new created one I could export without any error.

 

Regards

 

Chris

Re: STP export error

Siemens Phenom Siemens Phenom
Siemens Phenom

@Edifier_Chris , Yes, those issues were due to assembly file only while translating assembly. Glad to hear that problem is solved.

Regards,
Samadhan

GTAC | NX Help: NX1102 | NX1202 | NX1847
Please mark post as an "Accepted Solution", if it answers your question/is more helpful!