Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

STep file not Opening

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Dear All,

 

While opening the step file showing the following error. (NX 12.0.2)

 

Capture1.PNG

3 REPLIES 3

Re: STep file not Opening

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Atul3d,

Is this occurring specific to this file or for any STP/STEP file?

Regards,
Ganesh Kadole
#IngenuityIsNX | NX - What's New

Re: STep file not Opening

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Dear @GaneshKadole Sir,

This is file specific issue.

Following the LOg FILE TEXT.

 

>>>> Error code 1 caught in file "o:\ugnx1202\ip9\src\part\no\ind\part_foreign_step.c" at line number 964
Unloading C:\Program Files\Siemens\NX 12.0\nxbin\libap203.dll
>>>> Error code 1 caught in file "o:\ugnx1202\ip9\src\part\no\ind\part_foreign_step.c" at line number 1072
>>>> Error code 1 caught in file "o:\ugnx1202\ip9\src\part\no\ind\part_foreign.c" at line number 1568
Adding load status for C:\Users...................191072_00.stp - (1)

Load failed "C:\Users\......91072_00.stp": CPU time: 1.765 secs, Real time: 1.925 secs

&MACRO MESSAGE_BOX -2, Could not open C:\Users\Atul\Desktop\yeshree\trial\DU191072_00.stp.
&MACRO MESSAGE_TEXT The following files could not be loaded, causing this open to fail:
&MACRO MESSAGE_TEXT
&MACRO MESSAGE_TEXT C:\Users............072_00.stp - Error number: 1
&MACRO FILE_DIALOG_BEGIN 0, ! filebox with tools_data
&MACRO FILE_DIALOG_UPDATE 33
&MACRO FILE_DIALOG_END
&MACRO FILE_BOX -3,@@@ @@@@@@ 0 ! ##08Open
&MACRO SET_VALUE: 0 ! FSB item
&MACRO SET_VALUE: 0 ! FSB item
&MACRO MENU, 0, UG_HELP_SYSTEM_LOG UG_GATEWAY_MAIN_MENUBAR <RibbonTopBar->MenuBar->UG_HELP> ##

 

 

Hope sufficient for analysis....

Re: STep file not Opening

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Atul3d,

 

I would suggest reporting this to GTAC team.

 

Regards,
Samadhan

NX Help Links: NX1102 | NX1202 | NX1847
Please mark post as an "Accepted Solution", if it answers your question/is more helpful!