Cancel
Showing results for 
Search instead for 
Did you mean: 

Save Display Facets option in NX9

Pioneer
Pioneer

 

I have a part saved with "Save Display Facets" ON ( File>Preferences>Visualization Performance>General Graphics>Part Settings>Save Display Facets) .

 

 

If I turn it "OFF", and then save the part again, does it get rid of all the display facets already saved with the part?

 

If not, is there any other way of flushing/deleting all the display facet information saved with the part file?

 

Thanks!

1 REPLY

Re: Save Display Facets option in NX9

Siemens Phenom Siemens Phenom
Siemens Phenom

It appears that if all you do is toggled OFF this option, that nothing actually happens UNLESS the model had been updated before hitting the 'Save' button.  Now this can be as simple as either editing some feature, running the model Playback or else just editing some expression that updates the model and then edit it back to it's original value.  Then hit 'Save' and the facets will be removed, or at least it appears to work that way (I tested this checking the file size, using a very large and complex solid model, before and after toggling the option ON/OFF and with or without doing a model update).

John R. Baker, P.E. (ret)
EX-Product 'Evangelist'
Irvine, CA