Cancel
Showing results for 
Search instead for 
Did you mean: 

Save Failed Modeler error: irrecoverable run-time error

Experimenter
Experimenter

Hi guys,

I am running NX 9.0.2.5. I am having this error message come up every time I try to save this particular file. It allows me to save after running part cleanup sometimes, other times the session just freezes and never comes back after the error message.
What is causing this to pop up? I went though my features and removed all of the associative measures, and unparameterized features that didn't need to be associative, like lines and project curves etc.
There is nothing associative to this file in another external file.
I also attached a picture of the error.

Thanks for the help
Rob

2 REPLIES 2

Re: Save Failed Modeler error: irrecoverable run-time error

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You may have to send to GTAC for them to determine the issue.

Or upgrade to a newer version of NX.

Note NX9 may not be officially supported anymore.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Highlighted

Re: Save Failed Modeler error: irrecoverable run-time error

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Rob,

As suggested already GTAC will be the right option for you. In the mean time can you run an examine geometry check also... Also if your part has no more parametric features ...just copy it and paste it in another file and try saving the new part (or you can use EXPORT as part file ).

Best Regards

Kapil