Cancel
Showing results for 
Search instead for 
Did you mean: 

Save assembly load options - NX12

Creator
Creator

Hello all,

I usually use the "from search folders" to load assemblies.
Using the version 12, there are no option to save those configurations as default. So I have to recreate all anytime I reopen the user interface.

Can anyone help me with that?

Best regards,

Humberto

4 REPLIES

Re: Save assembly load options - NX12

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @HumbertoNaka,

I checked it. 'Save As Default', Reset 'Assembly Load Options' dilog then 'Restore Default' works absolutely fine in NX 12 (12.0.0.27 MP1). Are you able to save the defaults to 'load_options.def' file?

Re: Save assembly load options - NX12

Creator
Creator

I'm also using MP1, but those options are not visible in the Assembly load window.

I've attached an image to show it:

Assembly load options.png

I can't save nor load the .def file.

Best regards,

Humbert

Re: Save assembly load options - NX12

Siemens Phenom Siemens Phenom
Siemens Phenom

Set dilaog options to more so that it will show all the options for the respective dialog.asm.png

Re: Save assembly load options - NX12

Creator
Creator
Thanks Ganesh.

It was simple, but I could'nt find by myself...