Cancel
Showing results for 
Search instead for 
Did you mean: 

Scale imported stl file in NX

Experimenter
Experimenter

Hallo

 

I want to scale a body which I imported as a stl file. It didn't work with the normal "scale body" function. Is there a possibility to do it? And if yes, could you please tell me step by step what I need to do since I just started working with NX.

 

Thank you already in advance

thomafre

2 REPLIES 2

Re: Scale imported stl file in NX

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Menu -> edit -> transform, select STL body, choose "scale", specify a point to scale the body about, enter the desired scale factor, and in the final dialog, select "move" to transform the exisitng body or "copy" to create a new (scaled) body. Press "cancel" on the dialog to dismiss it after moving or copying the body.

Re: Scale imported stl file in NX

Experimenter
Experimenter
Amazing! Thank you very much.
Regards