Cancel
Showing results for 
Search instead for 
Did you mean: 

Scaling splines or sketch in modeling (feature and parameters)

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi there,

I have a simple question - as in topic - is there any way to easy scaling sketch/spline by using the base point with visible history of scaling parameter ?

 

For example:

I made one origin spline on deafult planar and second I made the copy on next planar. I want to transform this copied spilne by using 2:1 scale relative to the origin (know about edit>transform>scale>move). Only what I want to recive is History or Visible Parameter about the added scale . Many times I need to modify the previously scaled sketch.

========================================
Engineering >> NX10.0 Performance in the making
1 REPLY

Re: Scaling splines or sketch in modeling (feature and parameters)

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Unfortunately, there is no "scale curve" feature. However, there is a "scale body" feature; so one work-around would be to create an extrusion from the first curve, use scale body to apply the desired scale feature, and finally extract a curve from the edge of the resulting scaled body (or project the edge into a new sketch).