Cancel
Showing results for 
Search instead for 
Did you mean: 

Section in View (hidden)

Gears Phenom Gears Phenom
Gears Phenom

I just noticed that the "Section in View" command was hidden in my current set of tool bars, ie role.  I could add it without issue, but I generally start my role creation with "advanced, all menues".  So "Section in View" was either not included in the role I started with, OR it was hidden to get users using a new tool (based on past NX experience with things being hidden).

 

Is there a new and better tool, to select a component to be sectioned (or not sectioned) in a section view?

-Dave
NX 11 | Teamcenter 11 | Windows 10
2 REPLIES

Re: Section in View (hidden)

Phenom
Phenom

I use “Section View” instead of “Section in View”. It’s much more robust with Section Line Handles.

Michael Fernando


Die Designer
NX 11.0.2.7 + PDW

Re: Section in View (hidden)

Gears Phenom Gears Phenom
Gears Phenom

Seems to do the same thing, within the section view creation, instead of a secondary operation.  I guess I need to do more drawings!

 

Thanks

-Dave
NX 11 | Teamcenter 11 | Windows 10