Cancel
Showing results for 
Search instead for 
Did you mean: 

Section view - hidden lines

Builder
Builder

How to hide hidden lines in section view as default? And where is menu "Lock Alignment"  when create section view? Picture from NX9:

nx10-lock-alignment.jpg

NX10.0.3 MP03

8 REPLIES 8

Re: Section view - hidden lines

Master
Master

Not sure but look file/utilities/customer defaults/drafting/view

Shags72 Mfg. Eng.
Windows 10 Pro 64bit
NX 11.0.2.7 MP2 Teamcenter 11
Dell M7720 i7-6820HQ 16GB RAM,
NVIDIA Quadro P3000

Re: Section view - hidden lines

Builder
Builder

In file / utilities no options for section view - hidden lines.

Re: Section view - hidden lines

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Would they have buried that setting in the "drafting standard" section of the customer defaults?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Section view - hidden lines

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

I don't believe there is an option specifically for hidden lines in section views.

It can only be done after the view is created.

 

As for the lock alignment, change the placement to inferred and then you can "align to hinge" (see image below).

 

 

2016-04-19_15-10-31.jpg

Anthony Galante, Senior Support Engineer
PhoenxPLM
24 versions of NX installed: NX4 to NX12, plus TC11.2

Re: Section view - hidden lines

Builder
Builder

Thank you for your response. I was looking for something like "Align to Hinge".

In older version NX (9; 8.5; ...) section view was always created without hidden lines, independent of the base view.

sectionviewNX9.jpg

Re: Section view - hidden lines

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
The setting you've shown is a Common setting, meaning it applies to all view types, not just section views. NX10 is no different to the previous releases in that regard.
Anthony Galante, Senior Support Engineer
PhoenxPLM
24 versions of NX installed: NX4 to NX12, plus TC11.2

Re: Section view - hidden lines

Builder
Builder

There is a difference.

NX9

 

and NX10

 

When create section view from base view (with view hidden lines), I must always deactivate hidden lines. It is unnecessary clicks for me.

Re: Section view - hidden lines

Phenom
Phenom

 

I noticed that when creation of the section view, it follows the hidden line setting of the parent view. After creation of the section view, you could change the parent view hidden lines and the section view will not change its hidden lines. Anyhow too many clicks.

 

PS: In drafting standards (DIN ISO) it clearly state that NO HIDDEN LINES (unless really necessary) in the sectional views.

So if we are following standards, NX default should be this setting i.e No Hidden Lines in the section view. Unfortunately, we have to manually check and change it each time to follow the Standard.

Michael Fernando


Die Designer
NX 11.0.2.7 + PDW