Cancel
Showing results for 
Search instead for 
Did you mean: 

Selection of non visible items in full shaded view

Pioneer
Pioneer

In full shaded mode, during selection, it would be nice to have a partial transparent model near the selection area (let's say an improved Catia V5 way). This would be highly productive making easier to select non visible areas of the model.

Nowadays I can I input a ER?

 

4 REPLIES

Re: Selection of non visible items in full shaded view

Siemens Phenom Siemens Phenom
Siemens Phenom

Do you have Pre-selection Highlighting toggled 'ON'?  Also make sure that you have Edges Visible in Shaded views on as well.

John R. Baker, P.E. (ret)
EX-Product 'Evangelist'
Irvine, CA

Re: Selection of non visible items in full shaded view

Pioneer
Pioneer

Yes I do have Pre-selection Highlighting toggled 'ON' and Edges Visible in Shaded views.

For further insight please find attached the V5 way. I am shore that Siemens will be able to do it much better.

Is such affair eligible for a ER?

Re: Selection of non visible items in full shaded view

Siemens Phenom Siemens Phenom
Siemens Phenom

Yes, it's a reasonable candidate for an ER .

John R. Baker, P.E. (ret)
EX-Product 'Evangelist'
Irvine, CA

Re: Selection of non visible items in full shaded view

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Whether you can directly submit an ER, or whether you have to go thru a VAR, depends where/how you bought NX.

If you can, go this the GTAC site (https://www.plm.automation.siemens.com/en_us/support/gtac/) & select the"create or update an incident report" link

You might want to put in the IR text that you consider this to be an ER. 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled