Cancel
Showing results for 
Search instead for 
Did you mean: 

Selection tool in modeling

Creator
Creator

Dear All,

 

Since I work with NX (about 10 years) I have had this problem. Why does the selection tool not work like it should work?

When I want to select components which are inside the selection box it also selects components which are partly inside the box. And when I use crossing it does not select all the components that are crossing the box.

I also use the setting "no selection filter" and "entire assembly".

I find it always a lot of work to make good selections although it should be able to do it quickly if this function works properly. Really anoying.

 

Regards, Michel

NX10

3 REPLIES 3

Re: Selection tool in modeling

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Have you looked at the options in

Preferences -> Selection -> Selection rule...

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Selection tool in modeling

Siemens Phenom Siemens Phenom
Siemens Phenom

@MichelL

Are your assembly constraints displayed in the graphics window? I find that if a constraint falls within the rectangle selection, the component will be selected as well, however, if the constraint is hidden, then the same selection gesture will not select the unwanted component. See example below:

(view in My Videos)

Regards,
Abe

Re: Selection tool in modeling

Creator
Creator

In the preferences it is just the default value for inside and crossing etc. that can be changed.

 

I never display the assembly constraints.

 

I have added a video.