Cancel
Showing results for 
Search instead for 
Did you mean: 

Self-intersecting surface causes gap in solid

Experimenter
Experimenter

Hello,

 

We are trying to take a hex polygon and sweep it down a curve path.  When we do this it creates a gap in the resulting solid.  Has anyone worked around this before?

Self-Intersecting.png

 

Thanks!

 

Jim Mays

KUKA Assembly & Test

8 REPLIES

Re: Self-intersecting surface causes gap in solid

Gears Phenom Gears Phenom
Gears Phenom

Your bend radius is way to tight.  Visualize how that polygon sweeps around that fillet.  Your inside corners will self intersect.  You could sweep half of the polygon and model in the intersecting side using other commands.  make your bend radius larger will solve this issue.

Re: Self-intersecting surface causes gap in solid

Valued Contributor
Valued Contributor
Hi,
Could you please give a view without section cap?

Thx

Re: Self-intersecting surface causes gap in solid

Phenom
Phenom

@jmaize,

 

@sdetersis spot on - the reason that is happening is because the radius in the guide (bend) is too small and the hex surfaces on the inside of the bend (closest to the radius center) are collapsing on one another as you go around the radius. Increase the radius until the faces stop collapsing on themselves......OR

 

You can sort of simplify this by inscribing a circle around the hex points (the diameter touches the hex points) - make the bend radius equal to the radius of the circle - this will be the MINIMUM radius needed to successfully complete what you're doing. I will warn you, the inside bend (the side where you're seeing the faces collapse on each other) will be a sharp corner - you will need to increase the guide radius to have anything other than a sharp corner in this area.

hex bend.png

 

 We model lots of exhaust tubing and tube-like shapes and we usually have to at the very least a bend radius that is equal to the diameter of the tube (just for modeling purposes) - so if you use the example above, the diameter of the hex is 50 (2 X 25), so a bend radius of 50 would be fine - result shown below.

 

hex bend 2.png

-Tim

Re: Self-intersecting surface causes gap in solid

Gears Phenom Gears Phenom
Gears Phenom

 Just depends on what your end result needs to be.  I attached a really quick, different approach.  Done in NX11

 

 

 

 

Re: Self-intersecting surface causes gap in solid

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

@sdeters - you might want to run Examine Geometry on that part.

 

Regards, Ben

Re: Self-intersecting surface causes gap in solid

Gears Phenom Gears Phenom
Gears Phenom

thanks for pointing that out BenBroad.

 

Here is a better one.  Just a quick model.  It passes Examine.  Many ways to do this.  Using a sweep makes things really fun when modeling  swept surfaces, and extruded surfaces.  Very rough model once again.   

 

 

Re: Self-intersecting surface causes gap in solid

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

As previously pointed out, the self-intersection is to be expected.  You're going to have to reconsider the minimum radius as @TimF suggests, or look at modeling the part using different features as @sdeters suggests.  It's unfortunate that the Swept command cannot accomplish what you're attempting to do and to be honest I'm surprised it allowed the result (Sweep Along Guide raises an alert and does not allow the body to be created).  I've added a part created in NX 12 which required several more features than a single sweep to produce the same result.  As you know, there's probably many ways to resolve this (some more creative than others).

 

Regards, Ben

Re: Self-intersecting surface causes gap in solid

Phenom
Phenom
@BenBroad,

For the record, I used Sweep Along Guide - if all the sections and guides are lines and arcs, this is the perfect scenario for that command, IMO, and it will help prevent a novice user from making bodies with errors in them, as you more or less pointed out.
-Tim