10-18-2017 12:37 AM - edited 10-18-2017 12:38 AM
Hello!
I am getting 'Internal error: memory access violation' consistently for 'Send to Package File' command on NX 11.0.2.7 MP2.
However, on the same machine, it works fine with NX 10.0.3.5 MP19.
Thinking to report this issue to GTAC. Just want to check if this is version specific issue. It would be nice if someone help to check this command on NX 11.0.2.7 MP2.
Regards,
Ganesh
#IngenuityIsNX | NX - What's New
Solved! Go to Solution.
10-18-2017 02:06 AM
@GaneshKadole i have the same with NX11.0.2.7 mp2
When testing with NX12.0.0.26 it works fine.
There is already a call for this @ siemens (IR number 8994247)
10-18-2017 03:04 AM - edited 10-18-2017 03:05 AM
Thank you for the information!
I can see there is no solution/workaround information mentioned for that IR.
Copying and using the file 'pvtrans.dll' from MP1 seems to work. But is it really a preferred workaround/temporary solution (possibility of any consequences)?
Regards,
Ganesh
#IngenuityIsNX | NX - What's New
10-18-2017 03:09 AM
@GaneshKadole good to see that you have a workaround!
10-27-2017 12:35 PM - edited 10-27-2017 04:53 PM
Updated to NX 11.0.2.7 MP3 and this functionality is working fine.
Regards,
Ganesh
#IngenuityIsNX | NX - What's New