Cancel
Showing results for 
Search instead for 
Did you mean: 

Set a new configuration for Import Part

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi,

 

I'm working on NX Drafting and when I'm importing a part I need that the option for Layer automatically sets to Original:

unnamed.png

 

How can I set this? I've searched on the Customer Defaults and on the Drafting Preferences but haven't found the correct option.

 

 

 

 

3 REPLIES 3

Re: Set a new configuration for Import Part

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You should NOT be using the import -> part command to make a drawing of a part; this will create an independent copy of the geometry in your drafting part. Instead, the recommended practice is to add the model as a component in your drawing file (assemblies -> component -> add component), then switch to the drafting application to create and detail views of the part. By adding a component, you are referencing the model but not copying it. When the model gets updated, the drawing will update to reflect the changes.

Re: Set a new configuration for Import Part

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @gic_nx,

Use master model approach as @cowski1 mentioned already. After adding the component/assembly to the drawing part, you can check the layer option under the component properties. By default it will show the

'Original Layer'.asmlayer.png

 

Regards,
Ganesh Kadole
#IngenuityIsNX | NX - What's New

Re: Set a new configuration for Import Part

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Thank you both, I tried this but when I go to the Component Properties the default that is set to Layer Option is "No Change (Mixed)"

 

why is this?

 

thanks